News Releases

Mitsubishi Electric to Launch Large DIPIPM+ Series Simpler and more compact designs for inverter systems in air conditioners and industrial applications

FOR IMMEDIATE RELEASE No. 3280

TOKYO, May 7, 2019 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of three new Large DIPIPM+™ transfer-mold intelligent power modules featuring loading-converter circuits that realize simpler and more compact designs for use in air-conditioner and industrial inverters. Of special note, one of the new modules achieves a world's first* high-density output of 100A/1200V in its transfer-mold package. Sales of the new DIPIPM+ series will begin on May 29. Also, the modules will be exhibited at major trade shows, including Power Conversion Intelligent Motion (PCIM) Europe 2019 in Nuremberg, Germany from May 7 to 9 and PCIM-Asia 2019 in Shanghai, China from June 26 to 28.

  1. *According to Mitsubishi Electric research as of May 7, 2019

Mitsubishi Electric has been contributing to the miniaturization and energy-efficiency of inverter systems since commercializing its first DIPIPM™ series in 1997. The more compact and simpler-design DIPIPM+ series, which places the inverter and converter into one package, was introduced in 2015. In response to increasing demands for high-power compressors in package air conditioners, the company is now adding models of up to 100A/1200V for package (heat & cooling) air conditioners in the 56kW class.

New Large DIPIPM+ series

Sales Schedule

Product Model Specification Release date
Large DIPIPM+ series PSS50NE1CT 50A / 1200V May 29, 2019
PSS75NE1CT 75A / 1200V
PSS100NE1CT 100A / 1200V

Product Features

  1. 1) World's leading high-density output in transfer-mold package
    • PSS100NE1CT achieves a world's first high-density output of 100A/1200V in its transfer-mold package, suitable for 56kW class package air conditioners.
    • 100A/1200V model's small package and large capacity realized through Mitsubishi Electric's proprietary direct-wire-bonding technology
    • Built-in analog temperature voltage output and protection functions

  2. 2) Downsizing and simpler design for inverter systems
    • Built-in inverter, converter and drive circuits enable inverter systems with fewer external components
    • Simpler wiring pattern on board helps to downsize inverter systems

Note

Note that the press releases are accurate at the time of publication but may be subject to change without notice.


Inquiry

Media Contact

Customer Inquiries